Refresh SDK Repository Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Refresh SDK Repository Issue

Jump to solution
5,729 Views
oliviermonnom
Contributor II

Hi, 

I'm on Ubuntu 18.04 and since 2 days I've an issue when I open MCUXpresso IDE.

Once opened, the IDE (11.2.1) is doing a "Refresh SDK Repository..." and it takes full processing time (I see this with htop) until it crashes (internal error, see photo). I've downgraded to 11.1.1 (removing also all the config files from my home folder) and I have the same result.

I can't use anymore the IDE for my work! I can't figure out what is happening here.

My java version:

$ java -version
openjdk version "11.0.8" 2020-07-14
OpenJDK Runtime Environment (build 11.0.8+10-post-Ubuntu-0ubuntu118.04.1)
OpenJDK 64-Bit Server VM (build 11.0.8+10-post-Ubuntu-0ubuntu118.04.1, mixed mode, sharing)

Any help or advice welcome,

Thank you,

Olivier

0 Kudos
Reply
1 Solution
5,709 Views
oliviermonnom
Contributor II

Hi,

I did a new workspace in a new fresh folder but inside a git versioning folder -> same problem.

Then I did a new workspace in a new fresh folder outside this folder -> it worked.

Problem solved, thank you.

Olivier

View solution in original post

0 Kudos
Reply
2 Replies
5,722 Views
converse
Senior Contributor V

Suggest you post the log file:

<workspace>/.metadata/.log

Also, try starting MCUXpresso with a new, empty workspace.

0 Kudos
Reply
5,710 Views
oliviermonnom
Contributor II

Hi,

I did a new workspace in a new fresh folder but inside a git versioning folder -> same problem.

Then I did a new workspace in a new fresh folder outside this folder -> it worked.

Problem solved, thank you.

Olivier

0 Kudos
Reply