Redlink server and Windows 10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Redlink server and Windows 10

3,303件の閲覧回数
phateee
Contributor II

Hello,

Can somobeody help me?

I have Windows 10 and now I make new installation MCUXpresso V11. I have a problem with Redlink server.

pastedImage_1.png

I tried to do with V10. The problem is the same. When I install Windows 7, Redlink server goes without problem...

ラベル(1)
3 返答(返信)

3,100件の閲覧回数
converse
Senior Contributor V

Looks like your anti virus software is blocking the connection. Change the settings to allow red link server to establish connections.

0 件の賞賛
返信

3,100件の閲覧回数
phateee
Contributor II

I turned off antivirus and it doesnt work. Then I uninstalled antivirus and it doesnt work too.

0 件の賞賛
返信

3,100件の閲覧回数
converse
Senior Contributor V

Do you have the Windows Defender Firewall? You need to allow the redlinkserver application to have network access.

See the picture

Screenshot 2020-02-09 at 13.00.24.png

0 件の賞賛
返信