Redlink server and Windows 10

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Redlink server and Windows 10

2,437 Views
phateee
Contributor II

Hello,

Can somobeody help me?

I have Windows 10 and now I make new installation MCUXpresso V11. I have a problem with Redlink server.

pastedImage_1.png

I tried to do with V10. The problem is the same. When I install Windows 7, Redlink server goes without problem...

Labels (1)
3 Replies

2,234 Views
converse
Senior Contributor V

Looks like your anti virus software is blocking the connection. Change the settings to allow red link server to establish connections.

0 Kudos
Reply

2,234 Views
phateee
Contributor II

I turned off antivirus and it doesnt work. Then I uninstalled antivirus and it doesnt work too.

0 Kudos
Reply

2,234 Views
converse
Senior Contributor V

Do you have the Windows Defender Firewall? You need to allow the redlinkserver application to have network access.

See the picture

Screenshot 2020-02-09 at 13.00.24.png

0 Kudos
Reply