Hello,
I do flashing with "GUI Flash Tool" often with MCUXpresso and I need to select one of several connected boards.
Would it be possible to have any of the following features:
1. Save "Probes discovered" window size or change it's default width in any of the *.xml config files?
2. Save manually changed or automatically calculate "Available attached probes" columns width?
Best regards,
Piotr
Hi Erich,
Thx for good news.
Enough would be to know what to enter and in which .metadata\.plugins xml config file.
Best,
Piotr
To my understanding, these values are not stored anywhere (for now).
I had a hope these values are not stored but perhaps are read if available in config file.
It is OK, only one additional double click before each flashing.