Can't debug external memory resident rt1050 application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't debug external memory resident rt1050 application

1,607件の閲覧回数
BrianHBrook
Contributor I

We have two rt1050 evaluation boards modified to use qspi flash instead of the default hyper flash. One board was modified over a month ago and was fine until recently. One day, performance started to degrade in that the J-Link download dialog would repeatedly program the same area of flash before starting a debug session. Eventually it would fail altogether with something like

wont_start.jpg

It is also impossible to debug an application that is resident in the external DRAM, but it is possible to debug an application that completely sits in the internal RAM of the rt1050.

The second evaluation board was modified only days ago but showed this behavior from the beginning.

0 件の賞賛
返信
1 返信

1,534件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hello Brian,

I'd like to continue the support on your original thread, so we can keep the information in one place. 

https://community.nxp.com/thread/529267 

Best Regards,

Sabina

0 件の賞賛
返信