PNEV7462C examples don't debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PNEV7462C examples don't debug

ソリューションへジャンプ
3,179件の閲覧回数
Juergen_Abel
Contributor II

As a new developer in the field of NXP boards, I would like to test some sample programs for DESFire.
For the development board PNEV7462C I have added the examples from SW3683.zip to a new workspace, having "copy projects into workspace" unchecked during import.
The examples can be compiled without any error for debug configuration ReleasePN7462AU and for debug configuration DebugPN7462AU.
The PNEV7462C board is connected with the LPC-Link2 as shown in fig. 34 p. 32 of UM10883, both boards are connected via USB cables to a WINDOWS 10 pc.
VCOM drivers are installed, board is recognized as VCOM_PN7462AU.

The problem is, that when trying to debug a sample program, e.g. PN7462AU_exphExMain with debug configuration DebugPN7462AU, the process stops with errors listed below.

Is there any more config to be set in order to debug a sample program?


Cheers,

Juergen

#########################################################
Error message in "MCUXpresso IDE: Exception" dialog:
-----------------------------
IOExeption

Read timed out

Read timed out
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.receive(RedlinkServerClient.java:978)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1068)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1053)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.sendReceive(RedlinkServerClient.java:1040)
at com.nxp.mcuxpresso.core.debug.support.linkserver.redlink.client.RedlinkServerClient.wireConnect(RedlinkServerClient.java:1189)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.jtag.AbstractJtagDiscovery.ideConnect(AbstractJtagDiscovery.java:207)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.jtag.AbstractJtagDiscovery.connect(AbstractJtagDiscovery.java:187)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.jtag.AbstractJtagDiscovery.discover(AbstractJtagDiscovery.java:146)
at com.nxp.mcuxpresso.core.debug.support.linkserver.emulators.TargetDiscovery.jtagDiscovery(TargetDiscovery.java:445)
at com.nxp.mcuxpresso.core.debug.support.linkserver.launch.LaunchScriptUtils.getEmulatorInfo(LaunchScriptUtils.java:248)
at com.nxp.mcuxpresso.core.debug.support.linkserver.launch.LaunchScriptUtils.init(LaunchScriptUtils.java:488)
at com.nxp.mcuxpresso.core.debug.support.linkserver.launch.LaunchScriptUtils.<init>(LaunchScriptUtils.java:156)
at com.nxp.mcuxpresso.core.debug.support.linkserver.launch.LaunchScriptUtils.<init>(LaunchScriptUtils.java:143)
at com.nxp.mcuxpresso.core.debug.support.linkserver.services.TargetDiscoveryService.getTargetDiscovery(TargetDiscoveryService.java:138)
at com.nxp.mcuxpresso.core.debug.support.linkserver.override.LSFinalLaunchSequence$TargetDiscoveryJob.run(LSFinalLaunchSequence.java:124)
at org.eclipse.core.internal.jobs.Worker.run(Worker.java:63)

#########################################################
Error message in console log:
-----------------------------

MCUXpresso IDE RedlinkMulti Driver v11.5 (Dec 16 2021 12:38:31 - crt_emu_cm_redlink build 2)
Found part description in XML file PN74xxAU.xml
( 5) Remote configuration complete
Reconnected to existing LinkServer process.
Connecting to probe 1 core 0 (using server started externally) reports:
'Ee(42). Could not connect to core.'
Retrying...
Reconnected to existing LinkServer process.
Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.
============= SCRIPT: PN7xxxxx_Connect.scp =============
============= END SCRIPT ===============================
Failed on connect: Ee(42). Could not connect to core.
No connection to chip's debug port

 

0 件の賞賛
返信
1 解決策
3,168件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @Juergen_Abel :

 

I would suggest you update the firmware image.

Available firmware images include:

J-LINK On-board by Segger

CMSIS-DAP

Please try with J-LINK.

 

Please refer to below link for more details

https://www.nxp.com/design/microcontrollers-developer-resources/lpc-link2:OM13054

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,166件の閲覧回数
Juergen_Abel
Contributor II

Hello Daniel,
thanks for the hint, after programming the LPC-Link2 with Segger J-Link firmware, the sample programs run and debug.
Before, I have used the CMSIS-DAP firmware, which didn't work.

Cheers,
Juergen

0 件の賞賛
返信
3,159件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

thank you for your good news.

0 件の賞賛
返信
3,169件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @Juergen_Abel :

 

I would suggest you update the firmware image.

Available firmware images include:

J-LINK On-board by Segger

CMSIS-DAP

Please try with J-LINK.

 

Please refer to below link for more details

https://www.nxp.com/design/microcontrollers-developer-resources/lpc-link2:OM13054

 

0 件の賞賛
返信