Optimizing FreeRTOS NXP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Optimizing FreeRTOS NXP

4,769件の閲覧回数
trialaccount12
Contributor V

Hi,

        I am following the optimizing freeRTOS guide attached below. I have a few questions regarding it.

1. In section 4.1 , line 1 "Import the FRDM-K64F_SDK_FreeRTOS... ", which freeRTOS project it is referring to?

2. I tried using various freeRTOS programs like freeRTOS UART, but I could not see the list of TODO tasks as mentioned in step 5 of section 4. 

The dev board is FRDM - k64F.

Can someone help me with this?

Thanks and Regards

Niranjan

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

4,641件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

The example project selected is frdmk64f_freertos_generic.

I hope this helps, have a nice day!

Regards

Soledad

0 件の賞賛
返信

4,641件の閲覧回数
trialaccount12
Contributor V

Hi,

        yes, I have imported frdmk64f_freertos_generic.

But in section 4.1 , 

it says "Import the FRDM-K64F_SDK_FreeRTOS project found on the desktop", apparently this project has a list of TODO tasks mentioned. 

I can't find what project is this one?

Regards

Niranjan

0 件の賞賛
返信