NullPointerException in MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NullPointerException in MCUXpresso IDE

3,530 Views
kurt_staubli
Contributor III

I get often null pointer exception in MCUXpresso IDE 11.0.1.

I have to go through the following steps to reproduce it:

  • Open a project in MCUXpresso
  • Open a mex-file
  • Change perspective again to Develop
  • Open a different mex-file
  • Change perspective again to Develop
  • From now I get always java.lang.NullPointerException what ever I do
  • Workaround: Restart IDE or never open two different mex File inside MCUXpresso IDE
0 Kudos
Reply
4 Replies

3,376 Views
kurt_staubli
Contributor III

Hi Libor

You are corect: If I close Help, the exceptions vanishes. Thanks for the tip and good look in finding the culprit of the exception.

Regards,

Kurt

0 Kudos
Reply

3,376 Views
liborukropec
NXP Employee
NXP Employee

Hello Kurt,

you have probably opened the Help view in the Develop perspective. If you close it, the exceptions should stop showing (easier workaround then restarting IDE). We are looking for the root cause to fix it into the next version.

Regards,

Libor

0 Kudos
Reply

3,376 Views
kurt_staubli
Contributor III

Hi Alice

We are using RT1062.

Regards

Kurt

0 Kudos
Reply

3,376 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kurt Staubli,

Please tell me which chip do you used, I will check it  on my side.

BR

Alice

0 Kudos
Reply