NullPointerException in MCUXpresso IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NullPointerException in MCUXpresso IDE

3,603 次查看
kurt_staubli
Contributor III

I get often null pointer exception in MCUXpresso IDE 11.0.1.

I have to go through the following steps to reproduce it:

  • Open a project in MCUXpresso
  • Open a mex-file
  • Change perspective again to Develop
  • Open a different mex-file
  • Change perspective again to Develop
  • From now I get always java.lang.NullPointerException what ever I do
  • Workaround: Restart IDE or never open two different mex File inside MCUXpresso IDE
0 项奖励
回复
4 回复数

3,449 次查看
kurt_staubli
Contributor III

Hi Libor

You are corect: If I close Help, the exceptions vanishes. Thanks for the tip and good look in finding the culprit of the exception.

Regards,

Kurt

0 项奖励
回复

3,449 次查看
liborukropec
NXP Employee
NXP Employee

Hello Kurt,

you have probably opened the Help view in the Develop perspective. If you close it, the exceptions should stop showing (easier workaround then restarting IDE). We are looking for the root cause to fix it into the next version.

Regards,

Libor

0 项奖励
回复

3,449 次查看
kurt_staubli
Contributor III

Hi Alice

We are using RT1062.

Regards

Kurt

0 项奖励
回复

3,449 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kurt Staubli,

Please tell me which chip do you used, I will check it  on my side.

BR

Alice

0 项奖励
回复