MCUXpresso debugger when using an SREC file with Flash CRC inserted via srecord?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso debugger when using an SREC file with Flash CRC inserted via srecord?

Jump to solution
2,958 Views
med_engineer
Contributor I

I am working to add two 16-bit CRC values to our codebase at compile time in order to verify the integrity of the program text/data stored in flash memory and the text/data stored in QSPI.  I have managed to implement this functionality using srecord and the solution suggested in this NXP Community post. 

The problem is that this procedure does not integrate tightly with our standard build-compile-debug process in MCUXpresso.   I have been able to integrate the process with MCUXpresso by adding the Post-build steps shown below.  The three steps are to 1) copy the .axf file to a .srec file, 2) perform the CRC calculation and insertion at the proper addresses, and 3) Copy the .srec file back to a .axf file.

arm-none-eabi-objcopy -v -O srec "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.srec"


../program_crc/srecord-1.65.0-win64/bin/srec_cat.exe @../program_crc/srec_command.txt


arm-none-eabi-objcopy -v -I srec -O elf32-littlearm "${BuildArtifactFileBaseName}.crc.srec" "${BuildArtifactFileName}"

This works well in the sense that the build process is now entirely integrated with MCUXpresso.  However, the conversion from AXF to SREC and back again removes all of the debug information so that debugging is no longer possible.  

Has anyone been able to calculate and insert a CRC at compile time without losing all of the debug information stored in the AXF file?  There is a suggestion here which modifies the linker script.  However, MCUXpresso now uses managed linker scripts which I would like to maintain.  Is it possible to do this with templates?

 

Thanks for any suggestions!

FYI: we are using MCUXpresso v11.7.0 and developing for an MK82FN256 microcontroller.

0 Kudos
Reply
1 Solution
2,935 Views
ErichStyger
Specialist I

Hi @med_engineer ,

as for the linker script: did you know that you can use Freemarker to extend/modify it? I'm using it for example to build bootloaders, see https://mcuoneclipse.com/2019/10/06/linking-bootloader-applications-with-eclipse-and-freemarker-scri...

And you don't 'loose the debug information':

a) create a binary file from the .axf with the CRC inserted using SRecord

b) flash the binary file

c) debug with the symbols of the .axf (which has all the debug information)

You can tell the debugger not to flash, but to use the .axf for debug information, for example see

https://mcuoneclipse.com/2020/11/03/debugging-bootloader-and-application-with-one-debug-session/

I hope this helps.

View solution in original post

2 Replies
2,919 Views
med_engineer
Contributor I

@ErichStyger Thank you for the suggestion!  Your second suggestion to pull the symbols from the AXF file and the application code from the SREC file solved my issue.  Debugging is now completely seamless and works as one would expect.

Just to be clear for anyone else who sees this topic in the future; The steps below are what I had to do in MCUXpresso in order to implement this solution.

  1. Under the “Run” menu select “Debug configurations”
  2. Ensure that you have the correct debug configuration selected in the left-hand pane ("Sargasso_EFDemo JLink Debug” in the screenshots below).
  3. Under the “Main” tab, edit the “C/C++ Application” to use the SREC file using the “Browse” button (see screenshot below).
  4. Under the “Other Symbols” tab, edit the “Load symbols” file to point toward the AXF file using the “File System” button (see screenshot below).
  5. Click “Apply” to apply the new settings.

med_engineer_0-1692898969559.png

 

 

med_engineer_1-1692898969637.png

 

0 Kudos
Reply
2,936 Views
ErichStyger
Specialist I

Hi @med_engineer ,

as for the linker script: did you know that you can use Freemarker to extend/modify it? I'm using it for example to build bootloaders, see https://mcuoneclipse.com/2019/10/06/linking-bootloader-applications-with-eclipse-and-freemarker-scri...

And you don't 'loose the debug information':

a) create a binary file from the .axf with the CRC inserted using SRecord

b) flash the binary file

c) debug with the symbols of the .axf (which has all the debug information)

You can tell the debugger not to flash, but to use the .axf for debug information, for example see

https://mcuoneclipse.com/2020/11/03/debugging-bootloader-and-application-with-one-debug-session/

I hope this helps.