MCUXpresso 'FileNotFoundException' for crt_directory.xml (Access is denied)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso 'FileNotFoundException' for crt_directory.xml (Access is denied)?

6,299 次查看
jmreina
Contributor III

I am having file permissions problems with my project workspace that are unexpected -

 

Issue:

    Sometimes when I come into work to start a new day, the following occurs -

  • My workspace, or project within it gets corrupted and -
    • When MCUXpresso is opened a FileNotFoundException is thrown [Error_1]
    • The MCUXpresso Config Tool Perspectives stop working correctly
    • Issues with debug launches begin

    I also find this occurring periodically throughout the day, sometimes 5-6+ times!

 

Solution Found:

    I have burned lots of cycles trying to uncover! This works -

  • Switch to a new workspace
  • Copy-paste the project over to the new workspace & import into MCUXpresso

 

Notes:

  • New to MCUXpresso use (few weeks) & problem happens here consistently
  • Our organization has use of OneDrive which I have observed causing latency & access issues in other locations. The current workspace examples are outside of OneDrive's access now

 

What is causing this issue? Can it be fixed?

0 项奖励
回复
4 回复数

6,201 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jmreina 

1) How about disable firewall ?

2) What about the system you use?

 

BR

Alice

6,195 次查看
jmreina
Contributor III

Hi, this is a work machine and the firewall is required

Using Windows 10 Enterprise v22H2 on a Thinkpad P16 Gen 1

0 项奖励
回复

6,181 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @jmreina 

 

Because MCUXpresso IDE can works well on my side, and haven't encountered this kind of problem,

so recommend you some suggestions to check.

1) Just  want to check whether is the firewall problem. 

2) Also can try to re-install the IDE.

 

BR

Alice

 

 

BR

Alice

6,164 次查看
jmreina
Contributor III

This sounds great! Thank you for your feedback and advice Alice, I will give this a try and take notes

Back with response!

0 项奖励
回复