I am having file permissions problems with my project workspace that are unexpected -
Issue:
Sometimes when I come into work to start a new day, the following occurs -
I also find this occurring periodically throughout the day, sometimes 5-6+ times!
Solution Found:
I have burned lots of cycles trying to uncover! This works -
Notes:
What is causing this issue? Can it be fixed?
Hi, this is a work machine and the firewall is required
Using Windows 10 Enterprise v22H2 on a Thinkpad P16 Gen 1
Hello @jmreina
Because MCUXpresso IDE can works well on my side, and haven't encountered this kind of problem,
so recommend you some suggestions to check.
1) Just want to check whether is the firewall problem.
2) Also can try to re-install the IDE.
BR
Alice
BR
Alice
This sounds great! Thank you for your feedback and advice Alice, I will give this a try and take notes
Back with response!