LinkServer not Found

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LinkServer not Found

4,904 次查看
tkontogiorgis
Contributor II

Hello,

I am using W10 machine with LPCXpresso55S69 Board. I used the Board in another Windows 7 machine and everything was fine (also i used once in this Win10 machine and again fine!, maybe some windows updates caused the problem?  I cannot understand). I have a problem now with the Windows 10 machine while in Windows 7 machine i can 'see' the LinkSever. I am working with MCUXpresso IDE v11.1.1_3241 in both machines. I have the following problem:

pastedImage_1.png

1) I uninstalled and re-installed twice all the drivers and MCUXpresso IDE along with SDK's board.

2) I runned the boot_link2 (while the DFU was on)  and not solved:pastedImage_2.png

3) I tried to "Clean up Debug" via MCUXpresso IDE and re-run the debug but still nothing..

4) Tried to "Boot Debug Proble" ( with both DFU on and off)  via MCUXpresso IDE and this error occured:

pastedImage_3.png

pastedImage_4.png

5) Installed LPC_Scrypt v2.1.1_15 and run the lpc_driver_installer application and nothing changed.

6) Runned  program_CMSIS from LPCScrypt\Scripts path.Nothing happened..

All the clues show that is something probably with Windows 10 right? Is there anything else i could do? Unfortunately, i have only the Windows 10 engine available at the moment... 

0 项奖励
回复
5 回复数

4,776 次查看
tkontogiorgis
Contributor II

Hi converse‌,

After installing the MCUXpresso in another Windows 10 machine and working correctly i realized that the problem was specifically to my machine. I did 2 things in parallel so i don't know which of them solved the problem:

1) Uninstalled some latest Windows updates  ( KB4551762 and KB4540673) (I did this because some weeks ago

the specific machine was fully functional).

2) Uninstalled the MCUXpresso , all the windows drivers (these have been done again) and also after uninstalling

everything from Control Panel- Programms i deleted the Segger trash-remaining files that exist in Programm Files

even after uninstallation ( this was the first time i did that)

Now everything works!

Do you think the 2) (Segger remaining files in Programm Files could cause the problem? ) step should troubleshoot the problem or not? 

Best Regards,

Theo

4,776 次查看
tkontogiorgis
Contributor II

Hello converse‌ and thanks for the quick response,

1)i tried the following setup and nothing again.. ( 5V power Only from different machine and debug probe in the "problematic" machine):

IMG_8634.jpg

2) I also tried with another cable. Still nothing..

Sincerely,

Theo

0 项奖励
回复

4,776 次查看
tkontogiorgis
Contributor II

Hi converse‌

Thanks for responding,

pastedImage_2.png

The laptop has 3 Usb-ports (2 USB 2 and one USB 3.0). I tried to re-installed the USB Root Hub (not the Generic USB Hub) and nothing happened. Should i try to re-install the Generic USB Hub?

Best Regards,

Theo

0 项奖励
回复

4,776 次查看
converse
Senior Contributor V

No.

Have you tried connecting to a different USB port and have you tried a different USB cable? Are your USB ports able to supply sufficient power? If not, try external power

0 项奖励
回复

4,776 次查看
converse
Senior Contributor V

try running 

<xpresso_install>\ide\binaries\Scripts\listusb

and post the results

0 项奖励
回复