LibJPEG

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LibJPEG

2,023 次查看
mspenard603
Contributor IV

Hi All,

 I'm looking to use the LibJPEG available in the SDK middleware. But it needs a jconfig.h built. How do I build this for my iMXRT1062?

0 项奖励
回复
2 回复数

1,927 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hello Mike,

 

First, make sure you have MCUXpresso IDE 11.1 and SDK 2.7.0 installed.

 

Then, you can import our JPEG example project as follows.

pastedImage_1.png

Hope it helps!

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,927 次查看
mspenard603
Contributor IV

Also, how is FatFS typically tied into libjpeg? As libjpeg uses FILE file pointer structures, and Chan's FatFS uses its own FIL struct.

0 项奖励
回复