LPCOpen 2_12 for LPC11U68 bundle fixed and updated with FreeRTOSv9.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCOpen 2_12 for LPC11U68 bundle fixed and updated with FreeRTOSv9.0.0

2,033 次查看
fjrg76
Contributor IV

This is not a question but a way to share the little work I've done for such a bundle because I'll be using it a lot for the incoming months, and because I guess it may be of the interest for other programmers and enthusiasts, so no time is spent fixing and updating theirselfs what I've done.

As mentioned in this post the LPCOpen2_12 for the LPC11u68 is broken, so I tried to fix it, and I want to share with the community

 

My bundle includes 3 bundles:

  1. The original LPCOpen 2_12 fixed.
  2. LPCOpen 2_12 fixed, with FreeRTOSv9.0.0 and example in C.
  3. LPCOpen 2_12 fixed, with FreeRTOSv9.0.0 and example in C, besides some size optimizations in the libraries used (as long as you don't plan to debug such libraries) were exercised.

 

If there is other way to share my bundle other than this forum, please let me know it. Questions, bugs and comments are welcomed.

 

Kind regards.

Original Attachment has been moved to: lpcopen_2_12_lpcxpresso_nxp_lpcxpresso_11u68_fixed_by_fjrg76.zip

标签 (1)
0 项奖励
回复
2 回复数

1,876 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Javier,

 

Thanks for the contribution!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 项奖励
回复

1,876 次查看
fjrg76
Contributor IV

Any time!

0 项奖励
回复