MCUXpresso sh.exe crash cygwin error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso sh.exe crash cygwin error

ソリューションへジャンプ
2,963件の閲覧回数
ivaylomanushev
Contributor II

Hello All,

   I am having an issue every time I build my project I get an error that I shouldn't:

m.AllocationBase 0x0, m.BaseAddress 0x71110000, m.RegionSize 0x4C0000, m.State 0x10000
C:\nxp\MCUXpressoIDE_10.0.0_344\ide\msys\bin\sh.exe: *** Couldn't reserve space for cygwin's heap (0x71110000 <0x2930000>) in child, Win32 error 0

Now if I keep pressing the build button the project would compile after the 2nd or 3rd sometimes 4th consecutive build. 

Sometimes I would get a windows error that sh.exe has crashed with Fault Module Name: msys-1.0.dll

Any help in solving this issue would be appreciated!

Thanks,

Ivaylo

0 件の賞賛
返信
1 解決策
2,657件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Please see section 14.9, "Make fails with Virtual Alloc pointer is null error", of the MCUXpresso IDE v10.0.0 User Guide.

Regards,

MCUXpresso IDE Support

元の投稿で解決策を見る

2 返答(返信)
2,658件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Please see section 14.9, "Make fails with Virtual Alloc pointer is null error", of the MCUXpresso IDE v10.0.0 User Guide.

Regards,

MCUXpresso IDE Support

2,656件の閲覧回数
ivaylomanushev
Contributor II

Thanks for the info that worked like a charm!

0 件の賞賛
返信