IEC60730 lib integration problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IEC60730 lib integration problem

1,873 Views
AlperSefa
Contributor I

Hello,

While adding static lib IEC60730lib , i got some errors about it. Could you help what is the reason of this ?

 

Invoking: MCU Linker
arm-none-eabi-gcc -nostdlib -L"D:\xxx\safety\v4_1" -L"D:\xxx\safety\v4_1" -Xlinker -Map="xxx.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -Xlinker --sort-section=alignment -Xlinker --cref -mcpu=cortex-m7 -mfpu=fpv5-sp-d16 -mfloat-abi=hard -mthumb -T xxx_Debug.ld -L ../linker -o "xxx.axf" ./xip/evkmimxrt1020_flexspi_nor_config.o ./xip/fsl_flexspi_nor_boot.o ./utilities/fsl_debug_console.o ./utilities/fsl_str.o ./startup/startup_mimxrt1021.o ./source/yyy.o ./source/zzz.o ./source/ttt.o ./source/vvv.o ./source/bbb.o ./source/nnn.o ./source/mmm.o ./source/sss.o ./source/ddd.o ./source/fff.o ./source/ggg.o ./source/hhh.o ./source/hhh.o ./source/jjj.o ./source/kkk.o ./source/lll.o ./source/qqq.o ./source/www.o ./source/eee.o ./source/rrr.o ./safety/v4_1/wdog/iec60730b_wdog.o ./safety/safety_cm7_imxrt.o ./safety/safety_test_items.o ./drivers/fsl_clock.o ./drivers/fsl_common.o ./drivers/fsl_common_arm.o ./drivers/fsl_dmamux.o ./drivers/fsl_edma.o ./drivers/fsl_enc.o ./drivers/fsl_flexio.o ./drivers/fsl_flexio_uart.o ./drivers/fsl_gpio.o ./drivers/fsl_lpi2c.o ./drivers/fsl_lpi2c_edma.o ./drivers/fsl_lpuart.o ./drivers/fsl_lpuart_edma.o ./drivers/fsl_pwm.o ./drivers/fsl_qtmr.o ./drivers/fsl_tempmon.o ./drivers/fsl_wdog.o ./drivers/fsl_xbara.o ./device/system_MIMXRT1021.o ./component/uart/fsl_adapter_lpuart.o ./component/serial_manager/fsl_component_serial_manager.o ./component/serial_manager/fsl_component_serial_port_uart.o ./component/lists/fsl_component_generic_list.o ./board/board.o ./board/clock_config.o ./board/dcd.o ./board/peripherals.o ./board/pin_mux.o -lIEC60730B_M4_M7_MCUX_v4_1 -lIEC60730B_M4_M7_COM_MCUX_v4_1

ERROR:

d:/work/nxp/mcuxpressoide_11.5.1_7266/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.5.1.202201181444/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/bin/ld.exe: d:/work/nxp/mcuxpressoide_11.5.1_7266/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.5.1.202201181444/tools/bin/../lib/gcc/arm-none-eabi/10.3.1/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libcr_semihost_nf.a(_cr__main.o): in function `__main':

0 Kudos
Reply
2 Replies

1,805 Views
CarlosGarabito
NXP TechSupport
NXP TechSupport

Hi @AlperSefa which version of MCUXpresso are you using?, Which MCU are using?

0 Kudos
Reply

1,793 Views
AlperSefa
Contributor I

Hello,

 MCUXpresso IDE v11.5.1 [Build 7266] [2022-04-13]

 imxrt1021dag5a 

by the way i noticed i can build it in release mode, but i can't compile it in debug mode

@CarlosGarabito 

0 Kudos
Reply