I can not debug on FDRM KL25Z using MCUXpressoIDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I can not debug on FDRM KL25Z using MCUXpressoIDE

跳至解决方案
1,380 次查看
alejandra_flores18
Contributor I

I installed MCUXpressoIDE and the proper SDK's, I am using an old version FDRM KL25Z board, I connected it to my laptop with Windows 7 and it is recognized and seems like it has a precharged project with accelerometer because the color led changes according to positions, the green led is also blinking. My computer recognized the board as a device but in the device manager I have this...

Device managerDevice manager

The problem is that I can't debug any project, the error message is the following:

Error message at debugingError message at debuging

I have already updated the openSDA firmware with 118 version so now it is named BOOTLOADER but I can't debug yet. 

0 项奖励
回复
1 解答
1 回复
1,366 次查看
ErichStyger
Specialist I