I can not debug on FDRM KL25Z using MCUXpressoIDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I can not debug on FDRM KL25Z using MCUXpressoIDE

ソリューションへジャンプ
1,788件の閲覧回数
alejandra_flores18
Contributor I

I installed MCUXpressoIDE and the proper SDK's, I am using an old version FDRM KL25Z board, I connected it to my laptop with Windows 7 and it is recognized and seems like it has a precharged project with accelerometer because the color led changes according to positions, the green led is also blinking. My computer recognized the board as a device but in the device manager I have this...

Device managerDevice manager

The problem is that I can't debug any project, the error message is the following:

Error message at debugingError message at debuging

I have already updated the openSDA firmware with 118 version so now it is named BOOTLOADER but I can't debug yet. 

0 件の賞賛
返信
1 解決策
1 返信
1,774件の閲覧回数
ErichStyger
Specialist I