How to provide GDB options in LPCLink 2 Launch Config

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to provide GDB options in LPCLink 2 Launch Config

跳至解决方案
1,772 次查看
jschepler
Contributor III

I have run into the issue where breakpoints caused my code to stop working due to extended back tracing.

(Reference: https://community.nxp.com/thread/327560 )

I have successfully resolved the issue in the PEMicro Debugger Launch config.  It is very easy to add GDB commands in that dialog.

How do I go about adding these GDB options when debugging with an LPC Link 2? 

标记 (2)
0 项奖励
回复
1 解答
1,604 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

The issue you describe with backtrace causing debug problems is rather intriguing - I've certainly not come across anything similar to this previously.

But that aside, you can use the "Edit Scripts" button towards the bottom of the Debugger -> Target Configuration tab of the LinkServer Launch Configuration page to add the required gdb command.

Regards,

MCUXpresso IDE Support

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,605 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

The issue you describe with backtrace causing debug problems is rather intriguing - I've certainly not come across anything similar to this previously.

But that aside, you can use the "Edit Scripts" button towards the bottom of the Debugger -> Target Configuration tab of the LinkServer Launch Configuration page to add the required gdb command.

Regards,

MCUXpresso IDE Support

0 项奖励
回复
1,604 次查看
jschepler
Contributor III

Thank you for your prompt response, this resolved my issue. 

Here is an image showing the command added to the "Edit Scripts" dialog, and the command showing up in the GDB trace console when debugging:

LPCLink2BackTracePic.png

Yesterday I saw an area in the Debugger --> Main tab for a GDB command file.  It is currently empty.  I tried creating a file and adding the command there but it never worked. 

0 项奖励
回复