Hi Alexander,
Unfortunately, we do not recommend the creation of a project from scratch for Wireless Connectivity Products. The reason is that wireless examples do not depend completely on the SDK examples.
We recommend the usage of the current examples as a base and change only the application level of the examples.
We can recommend you to check the Connectivity Framework Reference Manual for some guidance of the linker file management, still, that would be the best we can help you.
"…\KW41_SDK\docs\wireless\Common\Connectivity Framework Reference Manual.pdf"
If you desire to develop for this IC with C++ it would be up to you the modifications and the development of the task.
If you use one of the basic examples linker files as a base, the linker file structure for those examples will be different from the wireless ones.
The MCUxpresso is based on Eclipse, that is the reason that supports the C++, but unfortunately, our setup and examples are not supported.
Sorry for the inconvenience this might cause you.
Regards,
Mario