Hello
I used for the first time MCUExpresso on the begining of this years (v11.1) on the Target processor KL02.
Today I start a new project based on the KL14Z84VFT4 and update IDE to v11.2
Then I start a new project, configure the Pin, the clock,
But for the perifpheral, to configure some basic thing to the ADC, UART, MCUExpresso IDE indicate to me the Peripherals tool is disable, in the Overview, section Peripheal, it is indicated "tool does not support selected processor".
It is a mistake from my project or it is realy impossible to generate the peripheral.c with this processor?
If it is impossible, where is the list of the supported processor?
Thank