How to add two or more SDK's on the same MCUXpresso workspace

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to add two or more SDK's on the same MCUXpresso workspace

ソリューションへジャンプ
2,745件の閲覧回数
MAPC
Senior Contributor I

I just tried to add FRDM-K64F KSDK to my workspace that already had OM13092 KSDK installed, but it fails.

Have you experienced something like that?

0 件の賞賛
返信
1 解決策
2,624件の閲覧回数
bryancole-b4682
NXP Employee
NXP Employee

Hi Marco,

Did you get an error message that you could share? 

Also, did you try to install the FRDM-K64F SDK package available from the Getting Started page?

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,625件の閲覧回数
bryancole-b4682
NXP Employee
NXP Employee

Hi Marco,

Did you get an error message that you could share? 

Also, did you try to install the FRDM-K64F SDK package available from the Getting Started page?

0 件の賞賛
返信
2,624件の閲覧回数
MAPC
Senior Contributor I

Hello, Bryan

My fault!

I just realized that I installed the wrong package. I corrected this and now it is working.

Thank you!

0 件の賞賛
返信
2,624件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Marco,

Which error are you getting? Please make sure the SDK package was created for the MCUXpresso toolchain.

Thanks in advance for your response!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信