How to add two or more SDK's on the same MCUXpresso workspace

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to add two or more SDK's on the same MCUXpresso workspace

Jump to solution
1,677 Views
MAPC
Senior Contributor I

I just tried to add FRDM-K64F KSDK to my workspace that already had OM13092 KSDK installed, but it fails.

Have you experienced something like that?

0 Kudos
1 Solution
1,556 Views
bryancole-b4682
NXP Employee
NXP Employee

Hi Marco,

Did you get an error message that you could share? 

Also, did you try to install the FRDM-K64F SDK package available from the Getting Started page?

View solution in original post

0 Kudos
3 Replies
1,557 Views
bryancole-b4682
NXP Employee
NXP Employee

Hi Marco,

Did you get an error message that you could share? 

Also, did you try to install the FRDM-K64F SDK package available from the Getting Started page?

0 Kudos
1,556 Views
MAPC
Senior Contributor I

Hello, Bryan

My fault!

I just realized that I installed the wrong package. I corrected this and now it is working.

Thank you!

0 Kudos
1,556 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Marco,

Which error are you getting? Please make sure the SDK package was created for the MCUXpresso toolchain.

Thanks in advance for your response!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos