Eclipse Marketplace/Installation of Eclipse plugins in MCUXpresso v11.9.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Eclipse Marketplace/Installation of Eclipse plugins in MCUXpresso v11.9.0

1,032 次查看
stefanct
Contributor IV

I'd like to install some plugins in MCUXpresso (v11.9.0) but every action I have tried in the Marketplace fails due to dependency problems, even the update of the existing Eclipe Marketplace Client (from 1.10.1 to 1.10.2).

For example the error for said update is this:

 

Cannot complete the install because of a conflicting dependency.
Software being installed: Marketplace Client 1.10.2.v20231116-1812 (org.eclipse.epp.mpc.feature.group 1.10.2.v20231116-1812)
Software currently installed: MCUXpresso IDE additional plugins 11.9.0.202401051634 (com.crt.lpcxpresso.feature.product.feature.group 11.9.0.202401051634)
Only one of the following can be installed at once:
Marketplace Client 1.10.1.v20221110-1841 (org.eclipse.epp.mpc.ui 1.10.1.v20221110-1841)
Marketplace Client 1.10.2.v20231116-1812 (org.eclipse.epp.mpc.ui 1.10.2.v20231116-1812)
Cannot satisfy dependency:
From: MCUXpresso IDE additional plugins 11.9.0.202401051634 (com.crt.lpcxpresso.feature.product.feature.group 11.9.0.202401051634)
To: org.eclipse.equinox.p2.iu; org.eclipse.epp.mpc.feature.group [1.10.1.v20221110-1841,1.10.1.v20221110-1841]
Cannot satisfy dependency:
From: Marketplace Client 1.10.1.v20221110-1841 (org.eclipse.epp.mpc.feature.group 1.10.1.v20221110-1841)
To: org.eclipse.equinox.p2.iu; org.eclipse.epp.mpc.ui [1.10.1.v20221110-1841,1.10.1.v20221110-1841]
Cannot satisfy dependency:
From: Marketplace Client 1.10.2.v20231116-1812 (org.eclipse.epp.mpc.feature.group 1.10.2.v20231116-1812)
To: org.eclipse.equinox.p2.iu; org.eclipse.epp.mpc.ui [1.10.2.v20231116-1812,1.10.2.v20231116-1812]

Similar issues arise when trying to install other plugins. This is observed on two different PCs (one Ubuntu, one Debian).

标记 (3)
0 项奖励
回复
1 回复

1,010 次查看
ErichStyger
Specialist I

I can conform that updating the marketplace plugin fails for me too.

But I had no issues so far installing other plugins so far.

So it might be related to that specific dependency. 

0 项奖励
回复