Eclipse Marketplace/Installation of Eclipse plugins in MCUXpresso v11.9.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Eclipse Marketplace/Installation of Eclipse plugins in MCUXpresso v11.9.0

952 Views
stefanct
Contributor IV

I'd like to install some plugins in MCUXpresso (v11.9.0) but every action I have tried in the Marketplace fails due to dependency problems, even the update of the existing Eclipe Marketplace Client (from 1.10.1 to 1.10.2).

For example the error for said update is this:

 

Cannot complete the install because of a conflicting dependency.
Software being installed: Marketplace Client 1.10.2.v20231116-1812 (org.eclipse.epp.mpc.feature.group 1.10.2.v20231116-1812)
Software currently installed: MCUXpresso IDE additional plugins 11.9.0.202401051634 (com.crt.lpcxpresso.feature.product.feature.group 11.9.0.202401051634)
Only one of the following can be installed at once:
Marketplace Client 1.10.1.v20221110-1841 (org.eclipse.epp.mpc.ui 1.10.1.v20221110-1841)
Marketplace Client 1.10.2.v20231116-1812 (org.eclipse.epp.mpc.ui 1.10.2.v20231116-1812)
Cannot satisfy dependency:
From: MCUXpresso IDE additional plugins 11.9.0.202401051634 (com.crt.lpcxpresso.feature.product.feature.group 11.9.0.202401051634)
To: org.eclipse.equinox.p2.iu; org.eclipse.epp.mpc.feature.group [1.10.1.v20221110-1841,1.10.1.v20221110-1841]
Cannot satisfy dependency:
From: Marketplace Client 1.10.1.v20221110-1841 (org.eclipse.epp.mpc.feature.group 1.10.1.v20221110-1841)
To: org.eclipse.equinox.p2.iu; org.eclipse.epp.mpc.ui [1.10.1.v20221110-1841,1.10.1.v20221110-1841]
Cannot satisfy dependency:
From: Marketplace Client 1.10.2.v20231116-1812 (org.eclipse.epp.mpc.feature.group 1.10.2.v20231116-1812)
To: org.eclipse.equinox.p2.iu; org.eclipse.epp.mpc.ui [1.10.2.v20231116-1812,1.10.2.v20231116-1812]

Similar issues arise when trying to install other plugins. This is observed on two different PCs (one Ubuntu, one Debian).

0 Kudos
Reply
1 Reply

930 Views
ErichStyger
Specialist I

I can conform that updating the marketplace plugin fails for me too.

But I had no issues so far installing other plugins so far.

So it might be related to that specific dependency. 

0 Kudos
Reply