Creating Flash Image for a 'Load from RAM' project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Creating Flash Image for a 'Load from RAM' project

2,389 次查看
Keith4DSmith
Contributor V

I am creating a program that runs in RAM using MCUXpresso and using Managed Linker Script. I check the 'Load from RAM' to create a program that runs exclusively in RAM.

Debugging the program is not a problem.

My question is there any NXP projects, supplied tools, or scripts to take the RAM image and attach it to a RAM loader to create an S-RECORD file that can be loaded into Flash. Thus on power-on the RAM image is loaded into RAM by the RAM loader and it jumps to the start of RAM.

标记 (1)
0 项奖励
回复
2 回复数

2,254 次查看
marek-trmac
NXP Employee
NXP Employee

Hi Keith,

for RT1050 and RT1060 you can use Secure Provisioning Tool. In the documentation you will find detailed description how to create bootable image.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 项奖励
回复

2,254 次查看
Keith4DSmith
Contributor V

Is the RT1060 option compatible with the RT1064?

0 项奖励
回复