Creating Flash Image for a 'Load from RAM' project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Creating Flash Image for a 'Load from RAM' project

2,384 Views
Keith4DSmith
Contributor V

I am creating a program that runs in RAM using MCUXpresso and using Managed Linker Script. I check the 'Load from RAM' to create a program that runs exclusively in RAM.

Debugging the program is not a problem.

My question is there any NXP projects, supplied tools, or scripts to take the RAM image and attach it to a RAM loader to create an S-RECORD file that can be loaded into Flash. Thus on power-on the RAM image is loaded into RAM by the RAM loader and it jumps to the start of RAM.

Tags (1)
0 Kudos
Reply
2 Replies

2,249 Views
marek-trmac
NXP Employee
NXP Employee

Hi Keith,

for RT1050 and RT1060 you can use Secure Provisioning Tool. In the documentation you will find detailed description how to create bootable image.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply

2,249 Views
Keith4DSmith
Contributor V

Is the RT1060 option compatible with the RT1064?

0 Kudos
Reply