Can't debug code link to RAM with Jlink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can't debug code link to RAM with Jlink

ソリューションへジャンプ
7,465件の閲覧回数
h_bouchard
Contributor III

I am using the rt1064 on a custom board (SDK version 2.9.1) and debugging using MCUXpresso IDE v11.3.0. I would like to link application to RAM but I'm not able to debug with Segger JLink Ultra+ probe.

To accomplish this, I did the following:

  • Set up SRAM_ITC to be the first RAM region listed in the memory configuration table (this region is large enough to hold our application).
  • Set up the SRAM_DTC to placed the heap and stack there.
  • Checked the "Link application to RAM" checkbox in the managed linker script.
  • In the Startup tab of the 'Edit Launch Configuration' dialog, set "monitor reset 6" to "Initialization Commands".
  • Remove XIP from SDK setup.
  • Remove XIP preprocessor defines from project settings.

When I try to download this through the debugger, the behavior is not stable. The first time I get this:

 

スポイラ

[26-2-2021 06:00:41] Executing Server: "C:\Program Files (x86)\SEGGER\JLink\JLinkGDBServerCL.exe" -nosilent -swoport 2332 -select USB=504505558 -telnetport 2333 -endian little -ir -speed auto -port 2331 -vd -device MIMXRT1064xxx6A -if SWD -halt -reportuseraction
SEGGER J-Link GDB Server V6.88c Command Line Version

JLinkARM.dll V6.88c (DLL compiled Dec 4 2020 18:05:56)

Command line: -nosilent -swoport 2332 -select USB=504505558 -telnetport 2333 -endian little -ir -speed auto -port 2331 -vd -device MIMXRT1064xxx6A -if SWD -halt -reportuseraction
-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: on
Silent mode: off
Single run mode: off
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: MIMXRT1064xxx6A
Target interface: SWD
Target interface speed: auto
Target endian: little

Connecting to J-Link...
J-Link is connected.
Device "MIMXRT1064XXX6A" selected.
Firmware: J-Link Ultra V4 compiled Nov 12 2020 10:07:39
Hardware: V4.00
S/N: 504505558
Feature(s): RDI, FlashBP, FlashDL, JFlash, GDB
Checking target voltage...
Target voltage: 3.30 V
Listening on TCP/IP port 2331
Connecting to target...
InitTarget() start
InitTarget()
_TargetHalt: CPU halted
InitTarget() end
Found SW-DP with ID 0x0BD11477
DPIDR: 0x0BD11477
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x04770041)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FD000
CPUID register: 0x411FC271. Implementer code: 0x41 (ARM)
Found Cortex-M7 r1p1, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
CoreSight components:
ROMTbl[0] @ E00FD000
ROMTbl[0][0]: E00FE000, CID: B105100D, PID: 000BB4C8 ROM Table
ROMTbl[1] @ E00FE000
ROMTbl[1][0]: E00FF000, CID: B105100D, PID: 000BB4C7 ROM Table
ROMTbl[2] @ E00FF000
ROMTbl[2][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7
ROMTbl[2][1]: E0001000, CID: B105E00D, PID: 000BB002 DWT
ROMTbl[2][2]: E0002000, CID: B105E00D, PID: 000BB00E FPB-M7
ROMTbl[2][3]: E0000000, CID: B105E00D, PID: 000BB001 ITM
ROMTbl[1][1]: E0041000, CID: B105900D, PID: 001BB975 ETM-M7
ROMTbl[1][2]: E0042000, CID: B105900D, PID: 004BB906 CTI
ROMTbl[0][1]: E0040000, CID: B105900D, PID: 000BB9A9 TPIU-M7
ROMTbl[0][2]: E0043000, CID: B105F00D, PID: 001BB101 TSG
Cache: Separate I- and D-cache.

I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way
D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
InitTarget() start
InitTarget()
_TargetHalt: CPU halted
InitTarget() end
Found SW-DP with ID 0x0BD11477
DPIDR: 0x0BD11477
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set)
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FD000
CPUID register: 0x411FC271. Implementer code: 0x41 (ARM)
Found Cortex-M7 r1p1, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
CoreSight components:
ROMTbl[0] @ E00FD000
ROMTbl[0][0]: E00FE000, CID: B105100D, PID: 000BB4C8 ROM Table
ROMTbl[1] @ E00FE000
ROMTbl[1][0]: E00FF000, CID: B105100D, PID: 000BB4C7 ROM Table
ROMTbl[2] @ E00FF000
ROMTbl[2][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7
ROMTbl[2][1]: E0001000, CID: B105E00D, PID: 000BB002 DWT
ROMTbl[2][2]: E0002000, CID: B105E00D, PID: 000BB00E FPB-M7
ROMTbl[2][3]: E0000000, CID: B105E00D, PID: 000BB001 ITM
ROMTbl[1][1]: E0041000, CID: B105900D, PID: 001BB975 ETM-M7
ROMTbl[1][2]: E0042000, CID: B105900D, PID: 004BB906 CTI
ROMTbl[0][1]: E0040000, CID: B105900D, PID: 000BB9A9 TPIU-M7
ROMTbl[0][2]: E0043000, CID: B105F00D, PID: 001BB101 TSG
Cache: Separate I- and D-cache.

I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way
D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
Connected to target
Waiting for GDB connection...Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0x00000000 (Data = 0x00000000)
Read 4 bytes @ address 0x00000000 (Data = 0x00000000)
Read 4 bytes @ address 0x00000000 (Data = 0x00000000)
Connected to 127.0.0.1
Reading all registers
Read 4 bytes @ address 0x00000000 (Data = 0x00000000)
Read 4 bytes @ address 0x00000000 (Data = 0x00000000)
Read 4 bytes @ address 0x00000000 (Data = 0x00000000)
GDB closed TCP/IP connection (Socket 1056)
GDB closed TCP/IP connection (Socket 1064)

Server has been shut down.

But the second time I try to debug I get this:

 

 

スポイラ

C:
xp\MCUXpressoIDE_11.3.0_5222\ide\plugins\com.nxp.mcuxpresso.tools.win32_11.3.0.202008311133 oolsinrm-none-eabi-gdb.exe: warning: Couldn't determine a path for the index cache directory.
GNU gdb (GNU Arm Embedded Toolchain 9-2020-q2-update) 8.3.1.20191211-git
Copyright (C) 2019 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law.
Type "show copying" and "show warranty" for details.
This GDB was configured as "--host=i686-w64-mingw32 --target=arm-none-eabi".
Type "show configuration" for configuration details.
For bug reporting instructions, please see:
<http://www.gnu.org/software/gdb/bugs/>.
Find the GDB manual and other documentation resources online at:
<http://www.gnu.org/software/gdb/documentation/>.

For help, type "help".
Type "apropos word" to search for commands related to "word"

 

 

The question is, am I missing any settings?

Thanks for your help!

Hugo

タグ(3)
1 解決策
7,413件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi h_bouchard,

I made a example which use jlink and run in sram. Please take a try.

 

Regards,

Jing 

元の投稿で解決策を見る

5 返答(返信)
7,441件の閲覧回数
nickwallis
Senior Contributor I

Hi,

You need to modify the debugger connect script (.SCP file) to reflect the changed flexRAM configuration. Did you do that?

-Nick

0 件の賞賛
返信
7,430件の閲覧回数
h_bouchard
Contributor III

Hi Nick,

Thanks for the reply but the flexRAM setting hasn't change therefore no need to modify .scp file.

Hugo

0 件の賞賛
返信
7,414件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi h_bouchard,

I made a example which use jlink and run in sram. Please take a try.

 

Regards,

Jing 

7,405件の閲覧回数
h_bouchard
Contributor III

Hello Jing,

Thank you so much for your help!!

As I expected, it was a debug configuration problem. The Initialize CPU registers checkbox was checked. Once unchecked, it worked fine.

Your the best !

Hugo

0 件の賞賛
返信
7,445件の閲覧回数
h_bouchard
Contributor III

I just tried with Ozone (Segger GUI for debugging) and I managed to start debugging my application. So the code is link to RAM properly.

It is most likely a faulty debug configuration. Does someone has managed to debug an application link to RAM with a JLink probe and MCUXpresso?

Thanks
Hugo

0 件の賞賛
返信