Build and re-flash while debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build and re-flash while debugging

1,607件の閲覧回数
bbenj
Contributor III

Hello,

I was wondering if it is possible to flash an MCU while running a debug session in MCUXpresso? Not having to stop the redlink server and restart a debug session every time I make a change would save me a lot of time, Eclipse is pretty slow...

I'm working with a i.MX RT 1021 & CMSIS-DAP, but I guess the option would work for any MCU?.

I searched the internet and Eclipse menus, but didn't find anything. I hope there's something I missed!

Thanks,

Best regards,

Benjamin

0 件の賞賛
返信
1 返信

1,537件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

MCUXpresso IDE does not support flash (re)programming while dealing with a live debug session. Flash is programmed only at the beginning of an actual debug session or as a completely separate action.

Greetings,
MCUXpresso IDE Support

0 件の賞賛
返信