BME688 sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BME688 sensor

2,028 Views
raduansarif
Contributor I

Hello, I am working with the BME688 sensor with MKL127LH4 processor and MCUxpresso ide, I2C communication interface. I could connect the MCU and BME688 sensor with I2C communication. But I cannot read the sensor data to print the temperature, pressure and gas. Actually, I don't understand which register address I need to use to access the data, what is the algorithm to access the data from the BME688 sensor. I will be thankful if anyone can help me by providing any tutorial or any I2C MCUxpresso example program for the BME688 sensor. Or is there any MCUxpresso I2C code for reading the sensor data?  Thank you.

0 Kudos
Reply
1 Reply

1,950 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

We don't have I2C demo code for  BME688 sensor.

But we can find general I2C communication demo code under MCUXpresso SDK folder. Users can refer it as a start stage to develop their dedicate I2C device drivers.

Thanks

Jun Zhang

 

0 Kudos
Reply