After programming with J-Link, the program cannot auto run.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

After programming with J-Link, the program cannot auto run.

4,223 Views
FanXH
Contributor II

I use MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13]

Jlink V7.66

After programming with J-Link, the program cannot auto run.I need to restart the development board manually.

FanXH_0-1666272066880.png

 

Thank you!

0 Kudos
Reply
5 Replies

4,207 Views
jay_heng
NXP Employee
NXP Employee

What is your MCU target?

0 Kudos
Reply

4,204 Views
FanXH
Contributor II

衡哥好!!!

RT1061

0 Kudos
Reply

4,200 Views
FanXH
Contributor II

When I click "Program flash action using SEGGER J-Link probes", it execute

FanXH_0-1666326720063.png

it should add a command "r" before "qc", it can auto run.

 

0 Kudos
Reply

4,132 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @FanXH, 

Could you try out to wait a little bit if it runs by itself? Checking your issue, there was a situation related with the time it gets to run after program the flash of the board.

Also, could you please check out that the RESET pin of the J-Link programmer is connected to the RESET pin of the board? Are you using a custom board?

Regards, Raul

0 Kudos
Reply

4,030 Views
FanXH
Contributor II

Yes, it can runs by itself after a long time, it seem 10s.

0 Kudos
Reply