Add binary file to a project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Add binary file to a project

2,190件の閲覧回数
MarcoGiammarini
Contributor III

Hello,

I would add to my project the binary file of the bootloader. In this way during board production, the operator can program the device only one time. Is there any way to do this?

Regards

Marco

0 件の賞賛
返信
3 返答(返信)

2,187件の閲覧回数
MarcoGiammarini
Contributor III

Hi @converse ,

thanks for your replay. Into my application, I want to add the binary image of the bootloader (It is a different project) at a specific address. In this way, I can generate during compilation only one file that includes the bootloader and application. At this time, the operator that program the board, do this operation only one time and not one time for bootloader and one time for application.

Regards

Marco 

0 件の賞賛
返信

2,174件の閲覧回数
converse
Senior Contributor V
0 件の賞賛
返信

2,188件の閲覧回数
converse
Senior Contributor V

I think you need to provide more information on what you are trying to do. What is the binary file? What are you expecting a bootloader to do with it?

0 件の賞賛
返信