Add binary file to a project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Add binary file to a project

1,547 Views
MarcoGiammarini
Contributor III

Hello,

I would add to my project the binary file of the bootloader. In this way during board production, the operator can program the device only one time. Is there any way to do this?

Regards

Marco

0 Kudos
Reply
3 Replies

1,544 Views
MarcoGiammarini
Contributor III

Hi @converse ,

thanks for your replay. Into my application, I want to add the binary image of the bootloader (It is a different project) at a specific address. In this way, I can generate during compilation only one file that includes the bootloader and application. At this time, the operator that program the board, do this operation only one time and not one time for bootloader and one time for application.

Regards

Marco 

0 Kudos
Reply

1,531 Views
converse
Senior Contributor V
0 Kudos
Reply

1,545 Views
converse
Senior Contributor V

I think you need to provide more information on what you are trying to do. What is the binary file? What are you expecting a bootloader to do with it?

0 Kudos
Reply