Add binary file to a project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Add binary file to a project

1,563 次查看
MarcoGiammarini
Contributor III

Hello,

I would add to my project the binary file of the bootloader. In this way during board production, the operator can program the device only one time. Is there any way to do this?

Regards

Marco

0 项奖励
回复
3 回复数

1,560 次查看
MarcoGiammarini
Contributor III

Hi @converse ,

thanks for your replay. Into my application, I want to add the binary image of the bootloader (It is a different project) at a specific address. In this way, I can generate during compilation only one file that includes the bootloader and application. At this time, the operator that program the board, do this operation only one time and not one time for bootloader and one time for application.

Regards

Marco 

0 项奖励
回复

1,547 次查看
converse
Senior Contributor V
0 项奖励
回复

1,561 次查看
converse
Senior Contributor V

I think you need to provide more information on what you are trying to do. What is the binary file? What are you expecting a bootloader to do with it?

0 项奖励
回复