I am using:
MCU-Link CMSIS-DAP V2.250
USB to Ethernet bridge: DS-510(from Silex)
IDE: Uvision Keil V5.37 & ARM DS 2022.1
The issue:
Connecting the MCU link to the PC is detectable by the IDE. But connect it via the bridge, it is not shown in the debugger list.
What I tried:
Using another CMSIS-DAP debugger works as expected with PC and bridge.
With a USB log view, there is no difference between connecting the MCU link via PC or via the bridge.
I notice that MCU-link creates 4 virtual ports while the other debugger( which worked) created only one port.