connecting MCU-link via USB-ethernet bridge

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

connecting MCU-link via USB-ethernet bridge

ソリューションへジャンプ
7,217件の閲覧回数
OussamaB
Contributor I

I am using:
MCU-Link CMSIS-DAP V2.250

USB to Ethernet bridge: DS-510(from Silex)

IDE: Uvision Keil V5.37 & ARM DS 2022.1

 The issue:

Connecting the MCU link to the PC is detectable by the IDE. But connect it via the bridge, it is not shown in the debugger list.

What I tried:
Using another CMSIS-DAP debugger works as expected with PC and bridge.
With a USB log view, there is no difference between connecting the MCU link via PC or via the bridge.
I notice that MCU-link creates 4 virtual ports while the other debugger( which worked) created only one port.

タグ(4)
0 件の賞賛
返信
1 解決策
7,187件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi OussamaB

I use MCU-Link on 64bit win10 computer. it can be well connected with MCUXpresso IDE.

Please follow below starting guide. If still can't work, change another computer, thus we can identify the problem is caused by your computer or other factors.

https://www.nxp.com/document/guide/getting-started-with-the-mcu-link:GS-MCU-LINK

Thanks,

Jun Zhang

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
7,183件の閲覧回数
OussamaB
Contributor I

Thanks,

With a direct connection between the MCU Link and the PC, it works as expected.

The issue was only with the USB-ethernet bridge.

But now with the MCUXpresso IDE, the probe is detectable via the bridge and has no issue.
So It looks like it is a Keil IDE issue. I will contact them.

Have a nice day  

0 件の賞賛
返信
7,188件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi OussamaB

I use MCU-Link on 64bit win10 computer. it can be well connected with MCUXpresso IDE.

Please follow below starting guide. If still can't work, change another computer, thus we can identify the problem is caused by your computer or other factors.

https://www.nxp.com/document/guide/getting-started-with-the-mcu-link:GS-MCU-LINK

Thanks,

Jun Zhang

0 件の賞賛
返信