USB Firmware update compatibility wrt LPC55s69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Firmware update compatibility wrt LPC55s69

ソリューションへジャンプ
7,847件の閲覧回数
Deeps_bang
Contributor III

hi Team,

 

"https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC54XXX-How-To-Use-USB-Port-To-Update-F..."

This article is useful and its wrt lpc54xxx.

We are working on LPC55s69 and planning to update firmware vis USB instead of ISP.

Is their any similar article/code project referencing LPC55s69 board.

If not, then can i use similar analogy as in article to implement  USB Firmware update for LPC55s69.

 

Thank you

0 件の賞賛
返信
1 解決策
7,785件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Deeps_bang 

I just checked runBootloader(arg) is supported in LPC55(S)0x/1x.

Unfortunately, LPC55(S)2x/6x doesn't support it. LPC55(S)2x/6x doesn't have feature to enter ISP mode in source code. So far there is no specific dates  to provide a procedure to  perform this.

There is an aplication note regarding this : AN12327  Firmware Update Using Secondary Bootloader

https://www.nxp.com.cn/docs/en/application-note/AN12327.pdf

You can refer this to development firmware update code with secondary bootloader.

Jun Zhang 

元の投稿で解決策を見る

0 件の賞賛
返信
12 返答(返信)
7,834件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Deeps_bang 

If LPC55, updating firmware via ISP USB is the same as this document.

But I suggset you using USB1 interface, the reason is documented here: https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC55-Don-t-Use-ISP-USB0-for-firmware-up...

Thanks,

Jun Zhang

 

0 件の賞賛
返信
7,812件の閲覧回数
Deeps_bang
Contributor III

HI Jennie,

  1. Our requirement is to enter Bootloader mode via USB , without using ISP Button for LPC55s69.

         which is best possible way to achieve this..?

    2.   Any suggestion for below issue ??

    In LPC54xxx -> iap_entry(API ) present in fsl_Flafhiap.h is used to reinvoke ISP.



     But in LPc55s69 -> No such API found in fsl_iap.h or fsl_iap.c. wrt SDK 2.12.0.

      so, how to achieve iap_entry() in LPC55s69??

 

Thank you.

 

 

0 件の賞賛
返信
7,832件の閲覧回数
Deeps_bang
Contributor III
Plz,Guide me to resolve this..

In LPC54xxx -> iap_entry(API ) present in fsl_Flafhiap.h is used to reinvoke ISP.



But in LPc55s69 -> No such API found in fsl_iap.h or fsl_iap.c. wrt SDK 2.12.0.

so, how to achieve iap_entry() in LPC55s69??
0 件の賞賛
返信
7,842件の閲覧回数
Deeps_bang
Contributor III

hi Team,

Any suggestion on this issue??

0 件の賞賛
返信
7,840件の閲覧回数
Deeps_bang
Contributor III

In LPC54xxx -> iap_entry(API ) present in fsl_Flafhiap.h  is used to reinvoke ISP.

 

But in LPc55s69 -> No such API found in fsl_iap.h or fsl_iap.c.  wrt SDK 2.12.0.

so, how to achieve iap_entry() in LPC55s69??

   

0 件の賞賛
返信
7,808件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Deeps_bang 

 ROMBootloader provides API  runBootloader to enter ISP mode.
void(*runBootloader)(void *arg);
 
For example, in your code, add:
uint32_t arg = 0xEB120000;
runBootloader(arg);
 
Hope this helps,
Jun Zhang
0 件の賞賛
返信
7,797件の閲覧回数
Deeps_bang
Contributor III

Hi Jennie,

Tried with runBootloader(arg).

But getting Hardfault error.

This (arg =0xEB120000) value corresponds to what .

we are using LPC55s69JBD100 board.

Attaching the code for your reference.

 

Thank you

0 件の賞賛
返信
7,733件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI Deeps_bang 
LPC55(S)2x/6x doesn't have feature to enter ISP mode in source code. LPC55(S)0x/1x has this feature but LPC55(S)2x/6x doesn't have. So far there is no specific dates to provide a procedure to perform this.

Have a nice day,
Jun Zhang

0 件の賞賛
返信
7,709件の閲覧回数
Deeps_bang
Contributor III

Hi Jennie,

Actually our application need this feature badly i.e Entering Bootloader mode via Software for LPC55s69JBD100 1B version board.

Please let me know if any update on this in Future from Technical team .

Mean while if any suggestions from your side for this problem statement is also welcome.

Thanks for guiding .

 

0 件の賞賛
返信
7,681件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

This feature is available on the newer version devices described in the errata:

https://www.nxp.com.cn/docs/en/nxp/errata/LPC55S6x_ES.pdf

ZhangJennie_0-1671436616383.png

To get ROM API version, you can call:

 

get_rom_api_version();

 

To get the ROM patch version, you can use blhost:

 

>blhost -p COMx get-property 0x18

 

The date code can be found in the IC package marking (See datasheet).

ZhangJennie_1-1671436802258.png

 

There is no way to apply a ROM patch by user, this is only done during production testing of the parts.

 

Hope this will help you.

Jun Zhang

0 件の賞賛
返信
7,786件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Deeps_bang 

I just checked runBootloader(arg) is supported in LPC55(S)0x/1x.

Unfortunately, LPC55(S)2x/6x doesn't support it. LPC55(S)2x/6x doesn't have feature to enter ISP mode in source code. So far there is no specific dates  to provide a procedure to  perform this.

There is an aplication note regarding this : AN12327  Firmware Update Using Secondary Bootloader

https://www.nxp.com.cn/docs/en/application-note/AN12327.pdf

You can refer this to development firmware update code with secondary bootloader.

Jun Zhang 

0 件の賞賛
返信
7,799件の閲覧回数
Deeps_bang
Contributor III
Ok Jennie.
Thank you for the reply.
I will try with this.
0 件の賞賛
返信