Redlib: where can I find the license doc for Redlib?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Redlib: where can I find the license doc for Redlib?

1,744 Views
erik_teose
Contributor I

[Hope my post goes to the right place.]

Subject line says it all: where is the license verbiage for Redlib? I'm running MCUXpresso IDE v11.0.0 [Build 2516] [2019-06-05]. Thanks!

0 Kudos
Reply
2 Replies

1,638 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Start off with looking at the "SoftwareContentRegister.txt" file inside the IDE installation directory.

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

1,638 Views
erik_teose
Contributor I

So Redlib is covered under "LA_OPT_TOOL Software Tools v14 January 2019; NXP SOFTWARE LICENSE AGREEMENT"? For some reason, I was under the impression that that agreement applied to components of the IDE itself (i.e. the stuff running on my development PC), and not to the object code that ends up in the target image I produce using the IDE. But upon closer examination of the agreement, it looks like it does cover "Compilable Software" which seems to include binary libraries. At least I think so.

0 Kudos
Reply