Processing:$01008000

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processing:$01008000

3,995件の閲覧回数
185206778
Contributor I

选好.s19程序文件后按Start,显示屏显示“Processing:$01008000”后就不动了, 是什么原因?怎么处理?

ラベル(1)
3 返答(返信)

3,852件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Guo,

Could you give us more information about the MCU and software being used?

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

3,851件の閲覧回数
185206778
Contributor I

Hi Carlos,

The used MCU is SPC5746RK1MMT5,where I use cyclone universal V9.80 as the automated programmer tool. After pressing the "Start" button,it displays processing:$01008000 few seconds later,and then nothing changed ablout 10 mins later.

How can fix this problem,Carlos?

Thanks.

3,851件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

in this case I recommend you to contact PEMicro support directly, because Cyclone universal is PEMicro product, so they can provide most accurate answer.

Regards,

Martin

0 件の賞賛
返信