Pin List - identifier warnings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin List - identifier warnings

1,504 Views
Beggar
Contributor I

Hello all,

Since I haven't filled the identifier column, I get a long list of "no identifier" warnings.

I want to get rid of them because I'm afraid to overlook more important warnings.

But I don't understand the concept of identifiers or what benefit they bring. I also don't understand why it is possible to assign multiple identifiers to one pin.

The minimal explanation in the user manual is not helpful. Can someone please point me to relevant documents or examples.

Thanks

0 Kudos
Reply
1 Reply

1,485 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Beggar,

Firstly, what user manual are you reffering to? I believe the User Guide for MCUXpresso Config Tools (Desktop) contains quite a bit of useful information about identifiers, including how to disable the warnings for "Not Specified" identifiers. As seen on 'Table 10. Preferences', option "Require Identifier for Pins (Pins Tool)" enables or disables the generation of warnings for pins with no related identifier:

ident_4.png

That said, identifiers can be very useful, specially when it comes to code congruency for the generated pin_mux files. As you can see on the following image, the identifier is only used as an 'alias' for the configuration structure used to initialized the pin on pin_mux.c (in this case, it only replaced gpio4_pinB1_config with SEMC_A6_config for congruency with the identifier "SEMC_A6"):

ident_1.png

However, on pin_mux.h, the change between no identifier and "SEMC_A6" is greater, since a whole set of macro definitions is generated according to the identifier (which before were inexistent before the identifier was defined):

ident_2.png

These macros are meant to be referenced during development of the application code to ensure congruency and standardize a naming convention for everything relating each defined pin. Defining multiple identifiers for each pin is also possible, but note that only one identifier can be used at once. This feature is basically only used to redefine all of the according macros at once (for example, changing "SEMC_A6" to "ID_TEST"):

EdwinHz_0-1705469991884.png

For more information regarding identifiers on ConfigTools, refer to section 3.3.4.2 Labels and identifiers on the aforementioned document.

BR,
Edwin.

0 Kudos
Reply