Good day,
I'm a engineer using PN7462AU. I am developing an NFC communication program. When I remove the card (tag), I want to recognize it and stop all communication.
Below is the setup details,
1. Hardware: PN7462AU
2. SDK: PN7462AU-FW_v05.21.00
3. IDE: MCUXpresso IDE v11.0.0
Question : Is there an API to immediately check if a card(tag) has been removed?
If anyone knows the answer to your question, please reply.
If you have any question, please feel free to contact me.
Thanks.
已解决! 转到解答。
Hello,
I believe the following code available in NfcrdlibEx4_MIFAREClassic example of the NFC Reader Library may help you. It is basically an infinite loop checking for card presence (WakeUpA and HaltA commands are sent continuously).
Code (NfcrdlibEx4_MIFAREClassic.c -> starting at line 305):
/* Make sure that example application is not detecting the same card continuously */
do
{
/* Send WakeUpA */
status = phpalI14443p3a_WakeUpA(pDiscLoop->pPal1443p3aDataParams,
pDiscLoop->sTypeATargetInfo.aTypeA_I3P3[0].aAtqa);
/* Check for Status */
if (status != PH_ERR_SUCCESS)
{
break; /* Card Removed, break from the loop */
}
/* Send HaltA */
status = phpalI14443p3a_HaltA(pDiscLoop->pPal1443p3aDataParams);
CHECK_STATUS(status);
/* Delay - 5 milli seconds*/
status = phhalHw_Wait(pDiscLoop->pHalDataParams, PHHAL_HW_TIME_MILLISECONDS, 5);
CHECK_STATUS(status);
}while(1);
Hope it helps!
BR,
Ivan.
Dear Ivan,
Thank you for response my question. I tried the code, but it didn't work. I think it didn't work by my mistake. I will contact you again if you have any further questions. Thank you.
Hello,
I believe the following code available in NfcrdlibEx4_MIFAREClassic example of the NFC Reader Library may help you. It is basically an infinite loop checking for card presence (WakeUpA and HaltA commands are sent continuously).
Code (NfcrdlibEx4_MIFAREClassic.c -> starting at line 305):
/* Make sure that example application is not detecting the same card continuously */
do
{
/* Send WakeUpA */
status = phpalI14443p3a_WakeUpA(pDiscLoop->pPal1443p3aDataParams,
pDiscLoop->sTypeATargetInfo.aTypeA_I3P3[0].aAtqa);
/* Check for Status */
if (status != PH_ERR_SUCCESS)
{
break; /* Card Removed, break from the loop */
}
/* Send HaltA */
status = phpalI14443p3a_HaltA(pDiscLoop->pPal1443p3aDataParams);
CHECK_STATUS(status);
/* Delay - 5 milli seconds*/
status = phhalHw_Wait(pDiscLoop->pHalDataParams, PHHAL_HW_TIME_MILLISECONDS, 5);
CHECK_STATUS(status);
}while(1);
Hope it helps!
BR,
Ivan.