MultiLink ACP with LPC microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MultiLink ACP with LPC microcontroller

2,755件の閲覧回数
kartheekgajjala
Contributor I

Does MultiLink ACP Rev B work with LPC micrcontrollers on MCUXpresso, I am having troubles flashing the chip. In the debug configurations on MCUXpresso, it recognizes the multilink as multilink ACP Rev B but keeps getting errors when trying to flash the chip. The errors are : 


Error! Enabling module timed out.
Error enabling module just selected.
Error loading programming algorithm - load aborted.
Error occured during Flash programming. 

I am 

0 件の賞賛
返信
2 返答(返信)

2,688件の閲覧回数
kartheekgajjala
Contributor I

Hey Steve,

The board is powered externally, I have tried both options of enabling/disabling "Use SWD protocol", neither works. The blue and orange LEDs are lit on the Multilink ACP. 

0 件の賞賛
返信

2,688件の閲覧回数
steven_mcgrath
Contributor II

Hello,

Are both the blue and orange LEDs lit on your Multilink ACP? How are you providing power, the Multilink ACP cannot provide power to the target device so the target device must be powered externally. Are you trying to connect via SWD protocol? If so, it looks like you have the “Use SWD protocol” checkbox unchecked which may be your issue.

Some things to consider, let me know if any of this information is helpful.

Steve

0 件の賞賛
返信