MKE04Z8VFK4 SDK overflow the program memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKE04Z8VFK4 SDK overflow the program memory

1,415 次查看
jingtian_li
Contributor II

Hello,

I tried to use the MKE04Z8VFK4 for build a project but the console showed the program memory was overflowed, the interesting thing was my project was empty, it contained nothing but pins and devices definitions.

So I created the new one which imported the examples (HelloWorld, UART_interrupt, UART_polling) of the SDK to see how they would be, they still showed the memory overflow, from 128%-140%.

Finally I created a empty project without any definitions but SDK, it still used 89.26% of program flash.

Anyone know how to reduce the size of the SDK significantly? Or the other ways which I can make the chip works? 10.74% is definitely not enough if I want to use the features of the chip.

My MCUXpresso is 11.1.0. SDK version 2.7.0 (Stage 736), Manifest Version 3.6.0. Config Tools 7.0.0

Thanks

make -r -j4 all
Building target: frdmke04z_sample_uart_polling.axf
Invoking: MCU Linker
arm-none-eabi-gcc -nostdlib -Xlinker -Map="frdmke04z_sample_uart_polling.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -Xlinker --sort-section=alignment -Xlinker --cref -mcpu=cortex-m0plus -mthumb -T frdmke04z_sample_uart_polling_Debug.ld -o "frdmke04z_sample_uart_polling.axf" ./utilities/fsl_assert.o ./utilities/fsl_debug_console.o ./startup/startup_mke04z4.o ./source/semihost_hardfault.o ./source/uart_polling.o ./drivers/fsl_clock.o ./drivers/fsl_common.o ./drivers/fsl_gpio.o ./drivers/fsl_port.o ./drivers/fsl_uart.o ./device/system_MKE04Z4.o ./component/uart/uart_adapter.o ./component/lists/generic_list.o ./board/board.o ./board/clock_config.o ./board/pin_mux.o
Memory region Used Size Region Size %age Used
PROGRAM_FLASH: 10564 B 8 KB 128.96%
c:/nxp/mcuxpressoide_11.1.0_3209/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.1.0.201909161352/tools/bin/../lib/gcc/arm-none-eabi/8.3.1/../../../../arm-none-eabi/bin/ld.exe: frdmke04z_sample_uart_polling.axf section `.text' will not fit in region `PROGRAM_FLASH'
c:/nxp/mcuxpressoide_11.1.0_3209/ide/plugins/com.nxp.mcuxpresso.tools.win32_11.1.0.201909161352/tools/bin/../lib/gcc/arm-none-eabi/8.3.1/../../../../arm-none-eabi/bin/ld.exe: region `PROGRAM_FLASH' overflowed by 2372 bytes
SRAM: 536 B 1 KB 52.34%
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:39: frdmke04z_sample_uart_polling.axf] Error 1
"make -r -j4 all" terminated with exit code 2. Build might be incomplete.

09:10:11 Build Failed. 3 errors, 0 warnings. (took 425ms)

标签 (1)
0 项奖励
回复
1 回复

1,304 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi jingtian,

printf occupies most of the code space. Please refer to Reduce source code size for Kinetis Series MKL03 

If space is still not enough, you can upgrade the compile optimize level. https://community.nxp.com/message/1053737?commentID=1053737#comment-1053737 

Regards,

Jing

0 项奖励
回复