The FlexPWM module can now capture the wrong channel, as can be seen in the figure below. So what should I do if I want to get the duty cycle waveform generated by FlexPWM? Is the capture function of the FlexPWM module or eTimer module used?
Hi,
unfortunately no figure is displayed.
Anyway the capture logic on PWMX input can be used for this.
You can refer e.g to https://community.nxp.com/message/1221963
BR, Petr