I cannot start debugging due to Debug Probe missing on LPC812MAX board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I cannot start debugging due to Debug Probe missing on LPC812MAX board

5,550 Views
seapon
Contributor I

I am using MCUXpressoIDE_10.3.1_2233 and installed SDK_2.x_LPCXpresso812MAX Sdk Ver.2.6.0 Manif Ver. 3.4.0 with LPCXpresso812MAX  FVB OM13055.

The project is the sample project _led_blinkly provided within SDK 2.6.

Of course, it can be built successfully.

However, [Debug]  select causes 

     1.  "unable to find dfu-util" message shows.

     2.  "no compatible probe available" shows.

     3.  Printer and Devices shows "MBED CMSIS-DAP" but not started

Like that, I cannot start load program to MCU nor start debugging.

By same IDE and PC environment, I made build and debugging for Kinetis successfully.

Please advice how to solve this.. 

0 Kudos
Reply
5 Replies

5,392 Views
lpcxpresso_supp
NXP Employee
NXP Employee

SDK 2.6.0 requires MCUXpresso IDE v11.0.0 or later.  And manually copying files from older IDE releases into an v11.0.0 install is definitely not supported or recommended !!!

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

5,392 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Masato Nishimoto,

- Please install the newer debugger firmware to your board refer to the below thread:

Flashing and Installing the new firmware and drivers for LPC11U35 debug probes    

- If you still want to use MBED, Certain mbed boards require a serial port driver to be recognised and this one exception
must be installed separately for each board. The driver is linked from Help -> Additional
Resources -> MBED Serial Port Driver Website

Windows serial configuration - Handbook | Mbed    


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

5,392 Views
seapon
Contributor I

Hello,Alice,

Thank you for your advice.

However, only update firmware LPC11U35 did not help to solve this.

I found that

 \MCUXpressoIDE_10.3.1_2233\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_10.3.1.201902111813\binaries

did not include any files othe than Flash, power, Scripts, ToolScripts.

If I might use MCUXprresso 11.0,this problem was solved. however new version did not work 32 environments.

So, I copied all files from older version and it was solved.

Can you agree that Ver 10.3.1_2233 have such problem and my solution is correct?

Best Regards,

Masato Nishimoto

0 Kudos
Reply

5,392 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Masato Nishimoto,

Thanks for your sharing.

Sorry I havn't 32 bits PC, and I checked my MCUXpressoIDE_10.3.1_2233 on 64 bits, 

under \nxp\MCUXpressoIDE_10.3.1_2233\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_10.3.1.201902111813\binaries includes  more files other than Flash. power, Scripts, , ToolScripts.

I think there is no problem you add these files by hand. 

0 Kudos
Reply

5,393 Views
seapon
Contributor I

Hallo, Alice,

Thank you for your advice.

However,only to update LPC11U35 firmware could not help this.

I found that \nxp\MCUXpressoIDE_10.3.1_2233\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_10.3.1.201902111813\binaries

includes NOTHING other than Flash. power, Scripts, , ToolScripts.

If I may use next version of MCUXpresso, but next one was ver 11.0 and it does not work on 32 environment.

..So, I copied other files which are included in older version to this version.

Do you agree that MCUXpressoIDE_10.3.1_2233 still have same problem and my repair for hat?

Best Regards,

Masato Nishimoto

0 Kudos
Reply