How to Disable RF

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Disable RF

5,820 Views
trivedimanva
Contributor II

Hi, 

I am working on the PN7462AU Eval Kit for the Contactless(CL) card & Contact(CT) card reader with "phExCcid" example.

And I need to switch OFF the RF and only need to ON the functionality for the Contact(CT) card only.

How can we switch OFF the RF functionality / field (I want to stop detecting the CL card) ?

Thanks in advance

Manva

Labels (1)
0 Kudos
Reply
9 Replies

5,584 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

Have you checked the phhalHw_FieldOff API ?You can see an example of its usage in the phExCcid_Clif.c file in the same example you are using.


Hope this helps.

Regards,

Estephania

0 Kudos
Reply

5,584 Views
trivedimanva
Contributor II

Hi estephania_martinez,

I tried your above mentioned API "phhalHw_FieldOff", But the RF field is still ON & it detects the CL card.

I am sharing screenshot were I have placed the API for your reference, If I am wrong & then please me know from where I have to call or place the API to switch OFF the RF-Field.

RF_API_REPLY_SCR_SHOT_2.PNG

I have called this function just before the CLIF function started in "phExCcid_ClifTask" function.

Looking forward for your feedback.

Thanks & Regards

Manva Trivedi

0 Kudos
Reply

5,584 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

Which is the process you want to follow ? Just to understand completely what you are trying to do

is it  Turn ON Field -> Detect CL card -> Turn Off field -> Detect CT card -> Repeat ?

 Which is your final application ?

Regards,
Estephania

0 Kudos
Reply

5,584 Views
trivedimanva
Contributor II

Hi estephania_martinez,

Which is your final application ?

-> I am using "phExCcid" example for my application. I need to switch OFF the RF and just run the CT interface only.

I need only CT operation & not CL operation. So I am looking for the deactivation RF in starting up code as you mentioned the steps.

I just want to use only CT functionality, not the CL from "phExccid" example.

Thanks & Regards

Manva Trivedi

0 Kudos
Reply

5,584 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

If you are not using the RF, have you tried not calling the initialization of the device?

Regards,
Estephania

0 Kudos
Reply

5,584 Views
trivedimanva
Contributor II

Hi estephania_martinez‌,

I already tried to do that but then after it goes to unknown state(say it hangs) and also stop detecting the CT card.

Can you please let know some another way to disable the RF field, through only CT will able to work.

Thanks & Regards

Manva Trivedi

0 Kudos
Reply

5,584 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

But if you are not using the RF, is there a specific reason why you are using that example ? You can check the PN7462AU_ex_phExCt and this might be easier for you to use and have the CT interface.


Regards,
Estephania

0 Kudos
Reply

5,584 Views
trivedimanva
Contributor II

Hi estephania_martinez‌,

I have gone through your suggested Example - "PN7462AU_ex_phExCt ", which for the simple polling for contact cards and the only difference is that they used transaction static predefined packets.

And they didn't used any read & Write functionality into it, Like in the "phExCcid" example. 

Even I have also gone through another example - "PN7462AU_ex_ phExCT7816", which is same nearly, Which is not support to my application.

I have to use SAM card for the my operation(RD/WR) with "phExccid" example.

That why I am using the "phExccid"-example for the application development.

So, Can you please share me the another way to switch OFF the RF field in "phExccid"-Example or if can share me any  Function or API through which I can switch of the Field properly.

Best Regards

Sachin

0 Kudos
Reply

5,584 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

Maybe you can try the stand by mode, please help me check this post to verify if this helps you

https://community.nxp.com/thread/453296 

Regards,
Estephania

0 Kudos
Reply