Error in final launch sequence

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error in final launch sequence

10,277 次查看
akshita_manwati
Contributor III

what is the meaning of error in final launch sequence and failed to execute MI command in MCUxpresso software for frdm KW36A board.

13 回复数

8,732 次查看
wangwenyu
Contributor II

NXP MCUXpresso is a bad IDE.

0 项奖励
回复

9,842 次查看
akshita_manwati
Contributor III

Hello

I am using version 10.3.0

Regards

Akshita

0 项奖励
回复

9,842 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

There is an issue with the new version of the MCUXpresso IDE and the Wireless Connectivity examples (including the KW36).

Meanwhile a new version of the IDE releases, could you please downgrade a version of the IDE so you can run the examples? 

Regards, 
Estephania 

0 项奖励
回复

9,842 次查看
nsuresh2
Contributor III

@Estephania Martinez

kw36‌ #mcuxpressoide_10.2.1_795‌
I am using MCUXpresso IDE v10.2.1 and still the same issue is seen in FRDM-KW36 

Error in final launch sequence
Failed to execute MI command:
-target-download
Error message from debugger back end:
Load failed
Load failed

Any other way to resolve this issue?

0 项奖励
回复

9,842 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Could you please help me attaching a screenshot of the issue? Also, just to confirm are you using the UART interface for debugging or are you using the semihosting option?  

Regards, 

Estephania 

0 项奖励
回复

9,842 次查看
nsuresh2
Contributor III

@Estephania Martinez

Hi,

Please check the below screenshots 

For Wireless_UART BLE example project I got the following error:

Default configuration:

default_config.png

Error:

w_uart.png

After changing the config:

config_changed.png

Error:

error.png

In both the case, the debugging option looks like this

debug_console.png

Semihost option is selected

proj_opt.png

0 项奖励
回复

9,842 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

That might be the root cause of your issue, could you please try debugging and deploying the firmware using the UART interface? Do you still get the errors? 


Regards, 

Estephania 

0 项奖励
回复

9,842 次查看
nsuresh2
Contributor III

estephania_martinez‌

Hi,

Once after changing it to UART interface it is working fine!

Thanks for your support!

Is there any option to change that setting from semihost to UART once after setting up the project using SDK import wizard

Because I could able to see that option only during import SDK examples (SDK import wizard)

Please let me know the steps to change it

Thanks!

0 项奖励
回复

9,842 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,  

 

Yes,  there is a way to do it either right-clicking the project or in the properties of it. 

 

Regards, 
Estephania 

0 项奖励
回复

9,842 次查看
nsuresh2
Contributor III

Hi estephania_martinez,

kw36‌mcuxpressoide_10.2.1_795 segger jlink #flexnvm‌

I am using Segger J-Link Plus debugger to download and debug the source code to KW36 board

For the Wireless_UART BLE example project 

  1. When I download the debug version of the project it is uploading properly

Whereas when I download the release version of the project it is showing the following error

Error in final launch sequence

Failed to execute MI command:

-target-select remote localhost:2336

Error message from debugger back end:

localhost:2336: No connection could be made because the target machine actively refused it.

localhost:2336: No connection could be made because the target machine actively refused it.

J-link error.png

2. When I try to write some data in the FlexNVM memory part it is not writing, please refer the below memory configuration

memory config.png

Thanks!

Regards,

Naven Suresh

0 项奖励
回复

9,842 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Could you please add this issue in a different thread?  This issue seems to be different also I will need more details on how you are deploying it, also, are you trying to debug the release version? Or are you just flashing it? 

Regards, 

Estephania 

0 项奖励
回复

9,842 次查看
nsuresh2
Contributor III

Hello,

Yeah Sure I will add this issue in a different thread.

I am just flashing the release version but I am not able to flash it 

0 项奖励
回复

9,842 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

Which version of McuXpresso are you working with ? 

Regards, 

Estephania

0 项奖励
回复