Error in FreeRTOS UART Example Application?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error in FreeRTOS UART Example Application?

跳至解决方案
2,551 次查看
myke_predko
Senior Contributor III

I'm following the TWRK21F "freertos_uart" example application and I just noticed that in the code, the setup/initial transmit APIs are written as:

if (0 > UART_RTOS_Init(&handle, &t_handle, &uart_config))
{
vTaskSuspend(NULL);
}

/* Send introduction message. */
if (0 > UART_RTOS_Send(&handle, (uint8_t *)to_send, strlen(to_send)))
{
vTaskSuspend(NULL);
}

In this code, the "vTaskSuspend(NULL); statements will only execute IFF the return value is less than zero (ie negative).  

When I look at the source code (in fsl_uart_freertos.c), the return values are defined (in fsl_common.h) as:

enum _generic_status
{
kStatus_Success = MAKE_STATUS(kStatusGroup_Generic, 0),
kStatus_Fail = MAKE_STATUS(kStatusGroup_Generic, 1),
kStatus_ReadOnly = MAKE_STATUS(kStatusGroup_Generic, 2),
kStatus_OutOfRange = MAKE_STATUS(kStatusGroup_Generic, 3),
kStatus_InvalidArgument = MAKE_STATUS(kStatusGroup_Generic, 4),
kStatus_Timeout = MAKE_STATUS(kStatusGroup_Generic, 5),
kStatus_NoTransferInProgress = MAKE_STATUS(kStatusGroup_Generic, 6),
};

As the return values will never be less than zero, won't the return tests for the APIs never become active? 

Shouldn't the first block of code be something like one of the two checks below?

if (0 != UART_RTOS_Init(&handle, &t_handle, &uart_config))  //  Not Equal to Zero
{
vTaskSuspend(NULL);
}

/* Send introduction message. */
if (UART_RTOS_Send(&handle, (uint8_t *)to_send, strlen(to_send)))  //  More Efficient way of detecting != Zero
{
vTaskSuspend(NULL);
}

0 项奖励
回复
1 解答
2,457 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi  Myke:

Thank you very much for your feedback. I will report this to the software team.

Regards

Daniel

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,458 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi  Myke:

Thank you very much for your feedback. I will report this to the software team.

Regards

Daniel

0 项奖励
回复