Enable external RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,262件の閲覧回数
Daan
Contributor III

In my project I use the RT1064 MCU with 1MB of on-board RAM. I have a 'simple' project with FreeRTOS/lwip enabled, I use the MQTT module of lwip. This all runs just fine. However, if I upscale my simple project with more functionalities, I notice the DTC_RAM gets over 100% full, so this will not run. However, we have 8MB of external RAM, so I'd like to use it. Unfortunately, I cannot get this to work, on startup, the code straightly runs to a hardfault. What am I doing wrong?

Please note the attachments for my configuration.

タグ(2)
0 件の賞賛
返信
1 解決策
7,249件の閲覧回数
Daan
Contributor III

It appears flex spi code has to implemented to get it working.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
7,250件の閲覧回数
Daan
Contributor III

It appears flex spi code has to implemented to get it working.

0 件の賞賛
返信